AssignDiscontinuityBuilderTypes Enumeration

NXOpen.Routing.AssignDiscontinuityBuilder.Types is an alias for NXOpen.Routing.AssignDiscontinuityBuilderTypes

class NXOpen.Routing.AssignDiscontinuityBuilderTypes

Bases: object

the Enum for the types Block

Enum Members

Enum Member Enum Member Description
Simple
Complex
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.