AlignStockBuilderStockAlignmentMethod Enumeration

NXOpen.Routing.AlignStockBuilder.StockAlignmentMethod is an alias for NXOpen.Routing.AlignStockBuilderStockAlignmentMethod

class NXOpen.Routing.AlignStockBuilderStockAlignmentMethod

Bases: object

Methods of aligning stocks.

Enum Members

Enum Member Enum Member Description
RoutingObject
VectorToVector
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.