RoughBrushFacetsRule Class¶
-
class
NXOpen.
RoughBrushFacetsRule
¶ Bases:
NXOpen.FacetSelectionRule
Represents a
NXOpen.FacetSelectionRule
that collects facets with rough brush tool intent.This rule expands to all neighboring facets of seed (and the neighbor-neighbors) that are inside or crossing brush tool. .. versionadded:: NX12.0.0
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the rough brush facets rule: NXOpen.RoughBrushFacetsRule |
Method Detail¶
Dispose¶
-
RoughBrushFacetsRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX12.0.0.
License requirements: None.
GetData¶
-
RoughBrushFacetsRule.
GetData
¶ Gets the data for the rough brush facets rule:
NXOpen.RoughBrushFacetsRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (roughBrushToolStartPoint, roughBrushToolDirection, roughBrushToolRadius, seedFacet) roughBrushToolStartPoint is a
NXOpen.Point3d
. the start point of rough brush tool roughBrushToolDirection is aNXOpen.Vector3d
. the vector defining direction of rough brush tool roughBrushToolRadius is a float. the radius of rough brush tool seedFacet is aNXOpen.IFacet
. the seed facet .. versionadded:: NX12.0.0License requirements: gateway (“UG GATEWAY”)