CommandImporter Class¶
-
class
NXOpen.Report.
CommandImporter
¶ Bases:
NXOpen.TransientObject
Represents a command importer to import the commands into command libary.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ImportOption | Returns or sets the command override option. |
Methods¶
Method | Description |
---|---|
Dispose | Destroys the object |
GetImportCandidates | Gets all candidate commands in library file. |
ImportCommands | Imports the selected commands into command library. |
Enumerations¶
CommandImporterOverrideOption Enumeration | Represents the override option when there is already a command existing. |
Property Detail¶
ImportOption¶
-
CommandImporter.
ImportOption
¶ Returns or sets the command override option.
-------------------------------------
Getter Method
Signature
ImportOption
Returns: Return type: NXOpen.Report.CommandImporterOverrideOption
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportOption
Parameters: importOption ( NXOpen.Report.CommandImporterOverrideOption
) –New in version NX11.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
CommandImporter.
Dispose
¶ Destroys the object
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetImportCandidates¶
-
CommandImporter.
GetImportCandidates
¶ Gets all candidate commands in library file.
Signature
GetImportCandidates()
Returns: Return type: list of NXOpen.Report.Command
New in version NX11.0.0.
License requirements: None.