PropertyContainerListMode Enumeration¶
NXOpen.PropertyContainer.ListMode is an alias for NXOpen.PropertyContainerListMode
-
class
NXOpen.
PropertyContainerListMode
¶ Bases:
object
Indicates whether the properties in the list are named.
Enum Members
Enum Member Enum Member Description Indexed The properties are not named and must be indexed through an integer index Named The properties are named -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-