ProeImporter Class¶
-
class
NXOpen.
ProeImporter
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.ProeImporter
to be used when importing the ProE Data This class is created usingNXOpen.DexManager
.NULL object will be returned from Commit() To create a new instance of this class, use
NXOpen.DexManager.CreateProeImporter()
Default values.
Property Value HealBodies 0 ImportTo WorkPart ImportToTeamcenter 0 IncludeNonManifoldObj 0 Optimize 0 SimplifyGeometry 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
HealBodies | Returns or sets the heal bodies - if set to true then imported data will be healed |
ImportTo | Returns or sets the import to. |
ImportToTeamcenter | Returns or sets the import to Teamcenter - if set to true then imported data can be added to Teamcenter |
IncludeNonManifoldObj | Returns or sets the include non manifold obj - if set to true then non-manifold objects from proe will also be imported |
InputFile | Returns or sets the input file - name of a file which is being imported |
Optimize | Returns or sets the Optimize - if value set to true then redundant geometries will be removed |
OutputFile | Returns or sets the output file - if proe file is imported to new part then this name will be used to write the output. |
SettingsFile | Returns or sets the settings file - definition file for default options |
SimplifyGeometry | Returns or sets the simplify geometry - if value set to true then imported data will be simplified |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SaveSettings | Save the settings - this will save the settings to a file specified |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ProeImporterImportToOption Enumeration | Import To Option |
Property Detail¶
HealBodies¶
-
ProeImporter.
HealBodies
¶ Returns or sets the heal bodies - if set to true then imported data will be healed
-------------------------------------
Getter Method
Signature
HealBodies
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HealBodies
Parameters: healBodies (bool) – New in version NX6.0.0.
License requirements: None.
ImportTo¶
-
ProeImporter.
ImportTo
¶ Returns or sets the import to.
This option will determine the destination for imported proe file. It can either be new part or work part.
-------------------------------------
Getter Method
Signature
ImportTo
Returns: Return type: NXOpen.ProeImporterImportToOption
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportTo
Parameters: importTo ( NXOpen.ProeImporterImportToOption
) –New in version NX11.0.0.
License requirements: None.
ImportToTeamcenter¶
-
ProeImporter.
ImportToTeamcenter
¶ Returns or sets the import to Teamcenter - if set to true then imported data can be added to Teamcenter
-------------------------------------
Getter Method
Signature
ImportToTeamcenter
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportToTeamcenter
Parameters: importToTeamcenter (bool) – New in version NX11.0.0.
License requirements: None.
IncludeNonManifoldObj¶
-
ProeImporter.
IncludeNonManifoldObj
¶ Returns or sets the include non manifold obj - if set to true then non-manifold objects from proe will also be imported
-------------------------------------
Getter Method
Signature
IncludeNonManifoldObj
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeNonManifoldObj
Parameters: includeNonManifoldObj (bool) – New in version NX6.0.0.
License requirements: None.
InputFile¶
-
ProeImporter.
InputFile
¶ Returns or sets the input file - name of a file which is being imported
-------------------------------------
Getter Method
Signature
InputFile
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InputFile
Parameters: filename (str) – New in version NX6.0.0.
License requirements: None.
Optimize¶
-
ProeImporter.
Optimize
¶ Returns or sets the Optimize - if value set to true then redundant geometries will be removed
-------------------------------------
Getter Method
Signature
Optimize
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Optimize
Parameters: optimize (bool) – New in version NX6.0.0.
License requirements: None.
OutputFile¶
-
ProeImporter.
OutputFile
¶ Returns or sets the output file - if proe file is imported to new part then this name will be used to write the output.
-------------------------------------
Getter Method
Signature
OutputFile
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFile
Parameters: filename (str) – New in version NX11.0.0.
License requirements: None.
SettingsFile¶
-
ProeImporter.
SettingsFile
¶ Returns or sets the settings file - definition file for default options
-------------------------------------
Getter Method
Signature
SettingsFile
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SettingsFile
Parameters: filename (str) – New in version NX6.0.0.
License requirements: None.
SimplifyGeometry¶
-
ProeImporter.
SimplifyGeometry
¶ Returns or sets the simplify geometry - if value set to true then imported data will be simplified
-------------------------------------
Getter Method
Signature
SimplifyGeometry
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SimplifyGeometry
Parameters: simplifyGeometry (bool) – New in version NX6.0.0.
License requirements: None.
Method Detail¶
SaveSettings¶
-
ProeImporter.
SaveSettings
¶ Save the settings - this will save the settings to a file specified
Signature
SaveSettings(filename)
Parameters: filename (str) – New in version NX6.0.0.
License requirements: None.
Validate¶
-
ProeImporter.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.