PrintPDFBuilderColor Enumeration¶
NXOpen.PrintPDFBuilder.Color is an alias for NXOpen.PrintPDFBuilderColor
-
class
NXOpen.
PrintPDFBuilderColor
¶ Bases:
object
Specifies the color option to use when creating the PDF document
Enum Members
Enum Member Enum Member Description AsDisplayed As Displayed PartColors Part Colors CustomPalette Custom Palette BlackOnWhite Black on White LegacyColors Legacy Colors ColorsByWidth Part Colors -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-