PrintPDFBuilderActionOption Enumeration¶
NXOpen.PrintPDFBuilder.ActionOption is an alias for NXOpen.PrintPDFBuilderActionOption
-
class
NXOpen.
PrintPDFBuilderActionOption
¶ Bases:
object
Specifies the action option to be used when running Teamcenter
Enum Members
Enum Member Enum Member Description New Create a new PDF document Overwrite Overwrite existing PDF document Append Append to existing PDF document Native Export to native folder -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-