PrintBuilderPaperSize Enumeration¶
NXOpen.PrintBuilder.PaperSize is an alias for NXOpen.PrintBuilderPaperSize
-
class
NXOpen.
PrintBuilderPaperSize
¶ Bases:
object
Specifies the paper size of the printed sheet
Enum Members
Enum Member Enum Member Description Letter 8 1/2- by 11-inches Legal 8 1/2- by 14-inches Inch9x11 9- by 11-inch sheet Inch10x11 10- by 11-inch sheet Inch10x14 10- by 14-inch sheet Inch15x11 15- by 11-inch sheet Inch11x17 11- by 17-inch sheet Inch12x11 12- by 11-inch sheet: Windows 98/Me, Windows NT 4.0 and later A2 A2 sheet, 420 x 594-millimeters A3 A3 sheet, 297- by 420-millimeters A3Extra A3 Extra 322 x 445-millimeters A3ExtraTransverse A3 Extra Transverse 322 x 445-millimeters A3Rotated A3 rotated sheet, 420- by 297-millimeters: Windows 98/Me, Windows NT 4.0 and later A3Transverse A3 Transverse 297 x 420-millimeters A4 A4 sheet, 210- by 297-millimeters A4Extra A4 sheet, 9.27 x 12.69 inches A4Plus A4 Plus 210 x 330-millimeters A4Rotated A4 rotated sheet, 297- by 210-millimeters: Windows 98/Me, Windows NT 4.0 and later A4Small A4 small sheet, 210- by 297-millimeters A4Transverse A4 Transverse 210 x 297 millimeters A5 A5 sheet, 148- by 210-millimeters A5Extra A5 Extra 174 x 235-millimeters A5Rotated A5 rotated sheet, 210- by 148-millimeters: Windows 98/Me, Windows NT 4.0 and later A5Transverse A5 Transverse 148 x 210-millimeters A6 A6 sheet, 105- by 148-millimeters: Windows 98/Me, Windows NT 4.0 and later A6Rotated A6 rotated sheet, 148- by 105-millimeters: Windows 98/Me, Windows NT 4.0 and later APlus SuperA/A4 227 x 356 -millimeters B4 B4 sheet, 250- by 354-millimeters B4JisRotated B4 (JIS) rotated sheet, 364- by 257-millimeters: Windows 98/Me, Windows NT 4.0 and later B5 B5 sheet, 182- by 257-millimeter paper B5Extra B5 (ISO) Extra 201 x 276-millimeters B5JisRotated B5 (JIS) rotated sheet, 257- by 182-millimeters: Windows 98/Me, Windows NT 4.0 and later B6Jis B6 (JIS) sheet, 128- by 182-millimeters: Windows 98/Me, Windows NT 4.0 and later B6JisRotated B6 (JIS) rotated sheet, 182- by 128-millimeters: Windows 98/Me, Windows NT 4.0 and later BPlus SuperB/A3 305 x 487-millimeters CSheet C Sheet, 17- by 22-inches DoubleJapanesePostcard Double Japanese Postcard, 200- by 148-millimeters: Windows 98/Me, Windows NT 4.0 and later DoubleJapanesePostcardRotated Double Japanese Postcard Rotated, 148- by 200-millimeters: Windows 98/Me, Windows NT 4.0 and later DSheet D Sheet, 22- by 34-inches Envelope9 #9 Envelope, 3 7/8- by 8 7/8-inches Envelope10 #10 Envelope, 4 1/8- by 9 1/2-inches Envelope11 #11 Envelope, 4 1/2- by 10 3/8-inches Envelope12 #12 Envelope, 4 3/4- by 11-inches Envelope14 #14 Envelope, 5- by 11 1/2-inches EnvelopeC5 C5 Envelope, 162- by 229-millimeters EnvelopeC3 C3 Envelope, 324- by 458-millimeters EnvelopeC4 C4 Envelope, 229- by 324-millimeters EnvelopeC6 C6 Envelope, 114- by 162-millimeters EnvelopeC65 C65 Envelope, 114- by 229-millimeters EnvelopeB4 B4 Envelope, 250- by 353-millimeters EnvelopeB5 B5 Envelope, 176- by 250-millimeters EnvelopeB6 B6 Envelope, 176- by 125-millimeters EnvelopeDl DL Envelope, 110- by 220-millimeters EnvelopeInvite Envelope Invite 220 x 220 mm EnvelopeItaly Italy Envelope, 110- by 230-millimeters EnvelopeMonarch Monarch Envelope, 3 7/8- by 7 1/2-inches EnvelopePersonal 6 3/4 Envelope, 3 5/8- by 6 1/2-inches ESheet E Sheet, 34- by 44-inches Executive Executive, 7 1/4- by 10 1/2-inches FanfoldUs US Std Fanfold, 14 7/8- by 11-inches FanfoldStandardGerman German Std Fanfold, 8 1/2- by 12-inches FanfoldLegalGerman German Legal Fanfold, 8 - by 13-inches Folio Folio, 8 1/2- by 13-inch paper IsoB4 B4 (ISO) 250- by 353-millimeters paper JapanesePostcard Japanese Postcard, 100- by 148-millimeters JapanesePostcardRotated Japanese Postcard Rotated, 148- by 100-millimeters: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeChou3 Japanese Envelope Chou #3: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeChou3Rotated Japanese Envelope Chou #3 Rotated: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeChou4 Japanese Envelope Chou #4: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeChou4Rotated Japanese Envelope Chou #4 Rotated: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeKaku2 Japanese Envelope Kaku #2: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeKaku2Rotated Japanese Envelope Kaku #2 Rotated: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeKaku3 Japanese Envelope Kaku #3: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeKaku3Rotated Japanese Envelope Kaku #3 Rotated: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeYou4 Japanese Envelope You #4: Windows 98/Me, Windows NT 4.0 and later JapaneseEnvelopeYou4Rotated Japanese Envelope You #4 Rotated: Windows 98/Me, Windows NT 4.0 and later Ledger Ledger, 17- by 11-inches LegalExtra Legal Extra 9 1/2 x 15 inches LetterExtra Letter Extra 9 1/2 x 12 inches LetterExtraTransverse Letter Extra Transverse 9 1/2 x 12 inches LetterRotated Letter Rotated 11 by 8 1/2 inches LetterSmall Letter Small, 8 1/2- by 11-inches LetterTransverse Letter Transverse 8 1/2 x 11-inches Note Note, 8 1/2- by 11-inches Prc16k PRC 16K, 146- by 215-millimeters: Windows 98/Me, Windows NT 4.0 and later Prc16kRotated PRC 16K Rotated, 215- by 146-millimeters: Windows 98/Me, Windows NT 4.0 and later Prc32k PRC 32K, 97- by 151-millimeters: Windows 98/Me, Windows NT 4.0 and later Prc32kRotated PRC 32K Rotated, 151- by 97-millimeters: Windows 98/Me, Windows NT 4.0 and later Prc32kBig PRC 32K(Big) 97- by 151-millimeters: Windows 98/Me, Windows NT 4.0 and later Prc32kBigRotated PRC 32K(Big) Rotated, 151- by 97-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope1 PRC Envelope #1, 102- by 165-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope1Rotated PRC Envelope #1 Rotated, 165- by 102-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope2 PRC Envelope #2, 102- by 176-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope2Rotated PRC Envelope #2 Rotated, 176- by 102-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope3 PRC Envelope #3, 125- by 176-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope3Rotated PRC Envelope #3 Rotated, 176- by 125-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope4 PRC Envelope #4, 110- by 208-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope4Rotated PRC Envelope #4 Rotated, 208- by 110-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope5 PRC Envelope #5, 110- by 220-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope5Rotated PRC Envelope #5 Rotated, 220- by 110-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope6 PRC Envelope #6, 120- by 230-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope6Rotated PRC Envelope #6 Rotated, 230- by 120-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope7 PRC Envelope #7, 160- by 230-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope7Rotated PRC Envelope #7 Rotated, 230- by 160-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope8 PRC Envelope #8, 120- by 309-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope8Rotated PRC Envelope #8 Rotated, 309- by 120-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope9 PRC Envelope #9, 229- by 324-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope9Rotated PRC Envelope #9 Rotated, 324- by 229-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope10 PRC Envelope #10, 324- by 458-millimeters: Windows 98/Me, Windows NT 4.0 and later PrcEnvelope10Rotated PRC Envelope #10 Rotated, 458- by 324-millimeters: Windows 98/Me, Windows NT 4.0 and later Quarto Quarto, 215- by 275-millimeter paper Statement Statement, 5 1/2- by 8 1/2-inches Tabloid Tabloid, 11- by 17-inches TabloidExtra Tabloid, 11.69 x 18-inches Custom Custom paper size, this requires the Custom Paper field to be set with the actual paper size ID -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-