PreviewPropertiesBuilderPartCreationOptions Enumeration¶
NXOpen.PreviewPropertiesBuilder.PartCreationOptions is an alias for NXOpen.PreviewPropertiesBuilderPartCreationOptions
-
class
NXOpen.
PreviewPropertiesBuilderPartCreationOptions
¶ Bases:
object
Specifies when the part preview will be created
Enum Members
Enum Member Enum Member Description OnSave Part preview will be created when the part is saved OnDemand Interactive only option that allows the part preview to be created by selecting the Create Now button -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-