SetPressModelBuilder Class
Properties
Property |
Description |
PressModelPartPath |
Returns or sets the file path to the press model root part |
Tag |
Returns the Tag for this object. |
Methods
Method |
Description |
Commit |
Commits any edits that have been applied to the builder. |
Destroy |
Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects |
For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject |
Returns the object currently being edited by this builder. |
ShowResults |
Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate |
Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail
PressModelPartPath