RotaryCamBuilder Class¶
Properties¶
Property | Description |
---|---|
BackstopOffset | Returns the offset (in degrees) from the cam to the backstop. |
CamAxis | Returns or sets the axis of rotation. |
CamBodies | Returns the rotary cam bodies. |
CamCollisionFacetingTolerance | Returns or sets the cam collision faceting tolerance. |
CompName | Returns or sets the unique name used to identify the simulation component. |
Description | Returns or sets the description of the cam. |
Disable | Returns or sets the disable status of the cam. |
DriveBodies | Returns the drive bodies. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
DeleteCam | To delete the cam. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetOutOfDate | To set the out of date status of the cam. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |