HydraulicLifterBuilderList Class
Properties
Property |
Description |
Length |
Returns the length of the list |
Tag |
Returns the Tag for this object. |
Methods
Method |
Description |
Append |
Appends a set of objects to the list |
Clear |
Clears the entire list without deleting the objects. |
ClearIndex |
Deletes the item at the index specified. |
Erase |
Erases the object from the list, but does not delete the object. |
FindIndex |
Finds the index where the input object appears. |
FindItem |
Returns the object at the input index. |
GetContents |
Gets the contents of the entire list |
Insert |
Inserts an object at the specified location |
MoveToBottom |
Move object at the specified location to the bottom of the list. |
MoveToTop |
Move object at the specified location to the top of the list. |
SetContents |
Sets the contents of the entire list. |
Swap |
Exchanges the position of two objects inside the list. |
Method Detail
Append
Clear
ClearIndex
Erase
FindIndex
FindItem
GetContents
Insert
MoveToBottom
MoveToTop
SetContents
Swap