HydraulicLifterBuilder Class
Properties
Property |
Description |
BackStopOffset |
Returns the backstop offset. |
CamBodies |
Returns the plunger bodies. |
CamCollisionFacetingTolerance |
Returns or sets the cam collision faceting tolerance. |
CamDir |
Returns or sets the cam direction. |
CompName |
Returns or sets the simulation component name. |
Description |
Returns or sets the description of the hydraulic lifter. |
Disable |
Returns or sets the disable status of the motion. |
DriveBodies |
Returns the plunger drive bodies. |
RamBodies |
Returns the ram bodies. |
RamDirection |
Returns or sets the ram motion direction. |
RamMaxLift |
Returns the ram maximum lift distance. |
RamToPlungerRatio |
Returns or sets the ratio that determines how far the the ram will move relative to the plunger. |
Tag |
Returns the Tag for this object. |
Methods
Method |
Description |
Commit |
Commits any edits that have been applied to the builder. |
DeleteCam |
To delete this motion. |
Destroy |
Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects |
For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject |
Returns the object currently being edited by this builder. |
SetOutOfDate |
To set the out of date status of the motion. |
ShowResults |
Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate |
Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail
BackStopOffset
CamBodies
CamDir
CompName
Description
Disable
DriveBodies
RamBodies
RamDirection
RamMaxLift
RamToPlungerRatio
Method Detail
DeleteCam
SetOutOfDate
Validate