AngleFormat Enumeration |
Specifies the view angle display format |
DecimalPointCharacter Enumeration |
Specifies the decimal point character for view angle display |
DetailBoundaryOption Enumeration |
Represents the boundary options |
Font Enumeration |
Represents the line font |
GdtOption Enumeration |
Represents the Inherit GD and T options |
GeneralDisplayIdOption Enumeration |
Represents the display id options |
GeneralExtractedEdgesOption Enumeration |
Represents the extracted edges options |
GeneralToleranceOption Enumeration |
Represents the General tolerance options |
GeneralViewLockmethodOption Enumeration |
Represents the view lock method options |
GeneralViewQualityOption Enumeration |
Represents the view quality options |
GeneralViewRepresentationOption Enumeration |
Represents the view representation options |
GeneralWireframeColorSourceOption Enumeration |
Represents the wireframe color source options |
HiddenLineInterferingSolidsOption Enumeration |
Represents the Interfering Solids options |
HiddenLineSmallFeatureOption Enumeration |
Represents the small feature options |
IncludeModelCurvesOption Enumeration |
Represents the include model curves options |
LoadDraftingStandardBuilderLoadLevel Enumeration |
This enum is for the load level |
ObjectPreferencesTranslucency Enumeration |
Describes whether the translucency is enabled or disabled |
PartDraftingBreakLineStyle Enumeration |
Describes the available break line style |
PartDraftingFontType Enumeration |
Describes the available font types |
PartDraftingUpdateViewWithoutLwDataOption Enumeration |
Describes the update view without light weight data options |
PartDraftingViewStyleType Enumeration |
Describes the available view style types for preview |
PartDraftingWidthType Enumeration |
Describes the available width types |
PartFlexiblePrintedCircuitDesignFlatPatternCalloutOrientationType Enumeration |
This enum represents orientation types for the flat pattern callouts |
PartFlexiblePrintedCircuitDesignFlatPatternObjectType Enumeration |
The members of the following enumerated type are used to identify object types to the FlatPattern API. |
PartFlexiblePrintedCircuitDesignFlexibleCableContactFaceOptions Enumeration |
This enum represents the face that is the contact face of the Flexible Cable. |
PartFlexiblePrintedCircuitDesignPlanarSegmentCurveType Enumeration |
The following members are used to identify curve types of planar segment feature. |
PartModelingCurveCurvatureDisplayType Enumeration |
Describes whether the curve curvature display is Curvature Comb or radius of Curvature Comb |
PartModelingDensityUnitType Enumeration |
Describes the units available for representing density |
PartModelingGridKnotLineFontType Enumeration |
the available font for grid/knot line |
PartModelingGridResolutionType Enumeration |
Describes all available grid resolutions for selection |
PartObjectColorSelection Enumeration |
Describes whether color of object is not changed or it is default color or it is defined by user |
PartObjectLineFontType Enumeration |
Represents the available types for font |
PartObjectObjectType Enumeration |
Describes all available Types for object selection |
PartObjectWidthType Enumeration |
Describes the available types for width |
PartSheetmetalBendDefinitionMethodOptions Enumeration |
This enum represents the bend definition method options in preferences. |
PartSheetmetalFlatPatternCalloutOrientationType Enumeration |
This enum represents orientation types for the flat pattern callouts |
PartSheetmetalFlatPatternObjectType Enumeration |
The members of the following enumerated type are used to identify object types to the FlatPattern API. |
PartSheetmetalTabCurveType Enumeration |
The following members are used to identify curve types of base tab feature. |
PartVisualizationColorSettingRandomColorDisplayFor Enumeration |
Describes whether the random color display is applicable for faces or bodies |
PartVisualizationEmphasisEdgesType Enumeration |
Determines whether or not edges are displayed for de-emphasized shaded geometry. |
PartVisualizationEmphasisSeeThruStyleType Enumeration |
Determines how translucency and color are used to de-emphasize shaded geometry. |
PartVisualizationLineLineFontDisplayType Enumeration |
Describes whether Line Font Display type is hardware or software. |
PartVisualizationNamesBordersNameDisplay Enumeration |
Describes the available options for object name display selection |
PartVisualizationScreenViewTriadLocation Enumeration |
The view triad location types. |
PartVisualizationShadeAdvViewToleranceType Enumeration |
Describes the available tolerance types for Advanced View. |
PartVisualizationShadeHiddenShadedFaceEdges Enumeration |
Describes whether the shaded face edges are invisible or dashed visible or with a color to depict the hidden geometry |
PartVisualizationShadeShadedFaceEdge Enumeration |
Describes whether the shaded face edges are having no color or body color or user defined color. |
PartVisualizationShadeShadedViewToleranceType Enumeration |
Describes the available tolerance types for Shaded View. |
PartVisualizationShadeViewUpdateModeType Enumeration |
Describes whether the applied changes are applicable to visible object or all object or no object |
PmiOption Enumeration |
Represents the Inherit PMI options |
ReferenceSetBehavior Enumeration |
Represents the Reference Set options |
RoutingApplicationViewAppType Enumeration |
Routing application types |
RoutingElectricalComponentMatchType Enumeration |
Manual/Auto Assign component uses the component match method to determine which component(s) are candidates for assignment to a component list record. |
RoutingElectricalCreateTerminalsType Enumeration |
How to create terminal segments (if creating terminal segments). |
RoutingLogicalFlowArrowEnumType Enumeration |
How to create terminal segments (if creating terminal segments). |
RoutingMechanicalLineColorType Enumeration |
Describes the Line color string definition types. |
RoutingPartDetailLevel Enumeration |
The detail levels available for the Routing bill of material. |
RoutingPartFabricationNumbering Enumeration |
The fabrication numbering methods available for the Routing bill of material. |
RoutingPartPreferredPortMethod Enumeration |
Available methods for determining which port is the preferredport during calculation of placement solutions. |
RoutingPartStockLengthDisplay Enumeration |
The stock length display options available for the Routing bill of material. |
RoutingPartUsePreferredPort Enumeration |
Whether or not use the preferred port when determining placement solutions. |
RoutingPartLibraryColumnStatus Enumeration |
Hidden status of a column. |
RoutingPartLibraryColumnType Enumeration |
Type of column values. |
RoutingPartLibraryNodeType Enumeration |
Type of nodes in the part library. |
RoutingPartLibraryRootType Enumeration |
Type of root nodes. |
RoutingPathAddPointsToSpline Enumeration |
Should points be added to existing spline when they are subdivided to preserve shape? |
RoutingPathAllowedCornerType Enumeration |
Describes the types of corners allowed in a routing application. |
RoutingPathChainMethod Enumeration |
Path curve chaining methods |
RoutingPathConfirmBranchSel Enumeration |
Should a branch selection confirmation dialog be show during Path selection? |
RoutingPathContinueUpdOnError Enumeration |
Should fixed length splines ignore length constraint violations and update? |
RoutingPathCreateSlopeConstraints Enumeration |
Create slope associativity constraints during line path creation [from ports only] |
RoutingPathCreateSmartRcps Enumeration |
Should Smart RCPs be created during path creation in Create Path? |
RoutingPathCreateTangency Enumeration |
Should new splines form tangencies with existing splines when they’re created? |
RoutingPathCurveType Enumeration |
Describes the types of curves allowed in a routing application. |
RoutingPathDefaultCornerType Enumeration |
Describes the types of corners allowed in a routing application. |
RoutingPathDisplayObject Enumeration |
Display a certain routing object? |
RoutingPathMergeDupRcps Enumeration |
Should duplicate RCPs be merged after a Transform [Move or Copy] operation? |
RoutingPathOccChainable Enumeration |
Chain occurrences of curves ? [i. |
RoutingPathRadiusMethod Enumeration |
Describes method used to determine bend radius on a bend or sbend corner |
RoutingPathRadiusUnits Enumeration |
Describes units of specified radius value NXOpen.Preferences.RoutingPathRadiusMethod.Radius only. |
RoutingStockSpaceReservationModeFlag Enumeration |
Describes the valid value for space reservation mode. |
RoutingStockStockModeFlag Enumeration |
Describes the valid value for stock mode. |
SessionAssembliesDragHandlePositionOption Enumeration |
Specify whether drag handle will be positioned at the center of bounding box or origin of component |
SessionAssembliesPartNameOption Enumeration |
Describe whether the part name style is file name or description or specified |
SessionAssembliesPositioningTaskCollectionOptionForDesignElements Enumeration |
Specify whether Design Elements will be added to the Work or Context Collection of a Positioning Task |
SessionDraftingAnnotationStyleType Enumeration |
Describes the available types for annotation style preference |
SessionDraftingEdgeFaceDisplayType Enumeration |
Describes the available edge face display types |
SessionDraftingGridObjectType Enumeration |
Describes the available grid objects |
SessionMeasureRequirementsActionOnViolation Enumeration |
Values for the action to take when a requirement error is generated for a measure with a displayed annotation in Assembly Sequencing. |
SessionModelingBodyTypeOption Enumeration |
Describes whether the body type is solid or sheet |
SessionModelingBooleanFacePropertiesInheritance Enumeration |
Describes whether the display of Boolean Face properties inherits from target body or tool body |
SessionModelingCurveFitMethodType Enumeration |
Describes whether the Curve Fit Method type is selected as cubic or quintic or advanced |
SessionModelingDeleteChildFeaturesOptionType Enumeration |
Options for controling delete child features, including recipe curves, of a feature being deleted |
SessionModelingDynamicUpdateType Enumeration |
Describes whether the Dynamic Update type is not selected or selected as incremental or continuous |
SessionModelingEndpointDisplayStyleType Enumeration |
Styles for display endpoints of curves |
SessionModelingFreeFormConstructionResultType Enumeration |
Describes whether the Free Form Construction Result is plane or B Surface |
SessionModelingImmediateChildrenType Enumeration |
Describes whether the Immediate Children type is selected for first level or for all |
SessionModelingLinkedAndExtractedGeometryPropertiesInheritance Enumeration |
Describes whether the display of linked and extracted geometry properties inherits from parent object or part default |
SessionModelingNewFacePropertiesInheritance Enumeration |
Describes whether the display of New Face properties inherits from body or part default |
SessionModelingPoleDisplayStyleType Enumeration |
Styles for display poles of B curves and B surfaces |
SessionModelingPoleEditStyleType Enumeration |
Styles for edit poles of B curves and B surfaces |
SessionModelingPolylineStyleType Enumeration |
Styles for polylines of B curves and B surfaces |
SessionModelingPreviewResolutionType Enumeration |
Freeform preview resolutions |
SessionModelingSaveDataForFeatureEditOption Enumeration |
Options for controling what additional data needs to be saved in part file to enhance the feature edit |
SessionModelingShareGeometriesOnSaveType Enumeration |
Options for saving a part file with sharing of geometry data to reduce file size |
SessionModelingSketchDefaultActionType Enumeration |
Double click action for sketches |
SessionModelingSketchEditType Enumeration |
Edit option for sketches |
SessionModelingSplineDefaultActionTypes Enumeration |
Specifies the command that should be invoked when double-clicking on a spline. |
SessionModelingSurfaceExtensionOption Enumeration |
Options for controling how surfaces will be extended while moving geometry |
SessionPdmJtUpdateFromSourceType Enumeration |
Options for the kind of JT update performed when a part is loaded |
SessionPdmMessagesInconsistentRevisionsType Enumeration |
Options for the kind of messages about inconsistent revisions when a part is loaded |
SessionPdmSynchroniseOnLoadType Enumeration |
Options for the kind of synchronisation with the PDM system performed when a part is loaded. |
SessionPdmSynchroniseOnSaveType Enumeration |
Options for the kind of synchronisation with the PDM system performed when a part is saved. |
SessionPdmUnpopulatedBehaviourType Enumeration |
Options for when to add NX datasets upon loading an unpopulated part in the PDM system |
SessionSketchBackgroundType Enumeration |
Describes the available sketch background types. |
SessionSketchGroupConstraintType Enumeration |
Represents the constraint management option when creating a rigid or scalable sketch group. |
SessionSketchOriginType Enumeration |
Describes the available sketch origin types. |
SessionSketchRigidSetConstraintType Enumeration |
Represents the constraint management option when creating a rigid sketch group. |
SessionUserInterfaceJournalFileFormatType Enumeration |
Describes the available format types for a journal file |
SessionUserInterfaceJournalLanguageType Enumeration |
Describes the language used to record journals |
SessionUserInterfaceUIDisplayResourceBar Enumeration |
Describes whether the resource bar is displayed on left or right of window |
SessionVisualizationHighEndRenderingMaterialEditorEditingMode Enumeration |
The two Studio Material Editor editing modes |
SessionVisualizationHighQualityImageImageSizeType Enumeration |
The size at which to generate a High Quality Image. |
SessionVisualizationHighQualityImageOrientationType Enumeration |
Whether the High Quality Image is to be generated with portrait or landscape orientation |
SessionVisualizationHighQualityImagePlotQualityType Enumeration |
Describes the quality desired when plotting the High Quality Image |
SessionVisualizationHighQualityImageResolutionType Enumeration |
The resolution to use when generating a High Quality Image. |
SessionVisualizationScreenViewTriadLocation Enumeration |
The view triad location types. |
SessionWorkPlaneObjectDisplay Enumeration |
Describes whether the object off work plane is normal display or dim and selectable or dim and non selectable |
ShadingRenderingStyleOption Enumeration |
Represents the rendering style options |
ShadingToleranceOption Enumeration |
Represents the Shade tolerance options |
ShipDraftingViewLinesViewPreferencesLines Enumeration |
Line type |
ShipbuildingLinesViewPreferencesLines Enumeration |
Line type |
ShipbuildingLinesViewPreferencesShipbuildingLines Enumeration |
Geometry type |
SketchPreferencesDimensionLabelType Enumeration |
Describes the different options for displaying dimension labels. |
SubdivisionModelingPreferencesCagePolylineVertexSizes Enumeration |
Cage polyline vertex size type. |
SubdivisionModelingPreferencesCagePolylineVertexStyles Enumeration |
Cage polyline vertex style. |
SubdivisionModelingPreferencesDisplayModes Enumeration |
Display modes of subdivision cage and resulting body. |
SubdivisionModelingPreferencesVertexSizeTypes Enumeration |
Vertex size type. |
SubdivisionModelingPreferencesVertexStyleTypes Enumeration |
Vertex display style. |
ViewVisualizationSpecialEffectsFogType Enumeration |
Describes whether the fog type is selected as linear or light or heavy. |
ViewVisualizationVisualDisplayModeType Enumeration |
Describes the available display mode types. |
ViewVisualizationVisualHiddenEdgeStyleType Enumeration |
Describes how hidden edges are displayed for shaded faces in the view. |
ViewVisualizationVisualHiddenEdges Enumeration |
Describes the appearance of hidden edges displayed in the view. |
ViewVisualizationVisualHiddenEdgesType Enumeration |
Describes the available hidden edges types. |
ViewVisualizationVisualRenderingStyle Enumeration |
Describes the rendering style for geometry displayed in the view. |
ViewVisualizationVisualShadedEdgeStyleType Enumeration |
Describes how edges are displayed for shaded faces in the view. |
ViewVisualizationVisualSmoothEdgeFont Enumeration |
Describes all possible font selection for visible smooth edges |
ViewVisualizationVisualSmoothEdgeWidth Enumeration |
Describes all possible width selection for visible smooth edges |
VisualizationFontsStyleType Enumeration |
Specifies the font style. |
VisualizationHandlesHandleSizeValue Enumeration |
Specifies size values for the default handle size. |
Width Enumeration |
Represents the line width |
WorkPlaneGrid Enumeration |
Describes whether the Grid type selected is Polar or Rectangular |