ViewVisualizationVisualSmoothEdgeWidth Enumeration

NXOpen.Preferences.ViewVisualizationVisual.SmoothEdgeWidth is an alias for NXOpen.Preferences.ViewVisualizationVisualSmoothEdgeWidth

class NXOpen.Preferences.ViewVisualizationVisualSmoothEdgeWidth

Bases: object

Describes all possible width selection for visible smooth edges

Enum Members

Enum Member Enum Member Description
Original
Thin
Normal
Thick
One
Two
Three
Four
Five
Six
Seven
Eight
Nine
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.