ViewVisualizationVisualHiddenEdgeStyleType Enumeration

NXOpen.Preferences.ViewVisualizationVisual.HiddenEdgeStyleType is an alias for NXOpen.Preferences.ViewVisualizationVisualHiddenEdgeStyleType

class NXOpen.Preferences.ViewVisualizationVisualHiddenEdgeStyleType

Bases: object

Describes how hidden edges are displayed for shaded faces in the view.

Enum Members

Enum Member Enum Member Description
Invisible
HiddenGeometryColor
Dashed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.