ViewVisualizationVisualDisplayModeType Enumeration¶
NXOpen.Preferences.ViewVisualizationVisual.DisplayModeType is an alias for NXOpen.Preferences.ViewVisualizationVisualDisplayModeType
-
class
NXOpen.Preferences.
ViewVisualizationVisualDisplayModeType
¶ Bases:
object
Describes the available display mode types. Specifies shading parameters for the selected view.
Deprecated since version NX4.0.0: Use
NXOpen.Preferences.ViewVisualizationVisualRenderingStyle
instead.Enum Members
Enum Member Enum Member Description Wireframe View is displayed as a wireframe-model PartiallyShaded Shade only selected object FullyShaded Shading is applicable to all objects in view FaceAnalysis Display faces using the color analysis data Studio In Studio mode, objects are realistically rendered according to material and texture characteristics assigned to them -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-