ViewVisualizationSpecialEffectsFogType Enumeration¶
NXOpen.Preferences.ViewVisualizationSpecialEffects.FogType is an alias for NXOpen.Preferences.ViewVisualizationSpecialEffectsFogType
-
class
NXOpen.Preferences.
ViewVisualizationSpecialEffectsFogType
¶ Bases:
object
Describes whether the fog type is selected as linear or light or heavy.
Enum Members
Enum Member Enum Member Description Linear Linear Fog Light Non linear Fog. Light fog produces a fog effect less pervasive than Heavy fog Heavy Non linear Fog -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-