ViewVisualizationSpecialEffectsFogData_Struct Struct¶
NXOpen.Preferences.ViewVisualizationSpecialEffects.FogData is an alias for NXOpen.Preferences.ViewVisualizationSpecialEffectsFogData_Struct
-
class
NXOpen.Preferences.
ViewVisualizationSpecialEffectsFogData_Struct
¶ Bases:
object
Represents the constituents of fog data .
Constructor: NXOpen.Preferences.ViewVisualizationSpecialEffects.FogData()
Fields¶
Field | Description |
---|---|
FogMode | Fog mode |
FogColorFlag | If true fog color is applied to the view |
FogColor | Fog Color |
FogStart | Start of fog |
FogEnd | End of fog |
FogDensity | Density of fog |
FogMode¶
-
ViewVisualizationSpecialEffectsFogData_Struct.
FogMode
¶ Fog mode
-------------------------------------
Field Value Type:int
FogColorFlag¶
-
ViewVisualizationSpecialEffectsFogData_Struct.
FogColorFlag
¶ If true fog color is applied to the view
-------------------------------------
Field Value Type:bool
FogColor¶
-
ViewVisualizationSpecialEffectsFogData_Struct.
FogColor
¶ Fog Color
-------------------------------------
Field Value Type:
NXOpen.Preferences.ViewVisualizationSpecialEffectsColorRGB_Struct
FogStart¶
-
ViewVisualizationSpecialEffectsFogData_Struct.
FogStart
¶ Start of fog
-------------------------------------
Field Value Type:float