SubdivisionModelingPreferencesDisplayModes Enumeration¶
NXOpen.Preferences.SubdivisionModelingPreferences.DisplayModes is an alias for NXOpen.Preferences.SubdivisionModelingPreferencesDisplayModes
-
class
NXOpen.Preferences.
SubdivisionModelingPreferencesDisplayModes
¶ Bases:
object
Display modes of subdivision cage and resulting body.
Enum Members
Enum Member Enum Member Description CageAndBody Display both cage and body CageOnly Display cage only BodyOnly Display body only -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-