SketchPreferencesDimensionLabelType Enumeration¶
NXOpen.Preferences.SketchPreferences.DimensionLabelType is an alias for NXOpen.Preferences.SketchPreferencesDimensionLabelType
-
class
NXOpen.Preferences.
SketchPreferencesDimensionLabelType
¶ Bases:
object
Describes the different options for displaying dimension labels.
Enum Members
Enum Member Enum Member Description Expression Displays the entire expression such as P2=P3*4 Name Displays only the name of the expression, such as P2 Value Displays the numerical value of the expression -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-