SessionVisualizationSpecialEffects Class¶
-
class
NXOpen.Preferences.
SessionVisualizationSpecialEffects
¶ Bases:
object
Represents the set of visualization special effect preferences applicable to entire session.
Set stereo preferences.
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
EnableStereo | Returns or sets the enable stereo flag. |
ParallaxFactor | Returns or sets the parallax factor. |
SupportStereo | Returns the support stereo flag. |
Methods¶
Property Detail¶
EnableStereo¶
-
SessionVisualizationSpecialEffects.
EnableStereo
¶ Returns or sets the enable stereo flag.
Toggles the display of stereo. To see correct stereo display, you need a supported graphics card, a 3D Stereo Display or Projector, and 3D glasses (and possibly a hub). The hardware vendor control panel Stereo option must also be turned on.
-------------------------------------
Getter Method
Signature
EnableStereo
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnableStereo
Parameters: enableStereo (bool) – New in version NX9.0.0.
License requirements: None.
ParallaxFactor¶
-
SessionVisualizationSpecialEffects.
ParallaxFactor
¶ Returns or sets the parallax factor.
Defines the amount of ‘Stereo effect’. A larger setting produces stronger 3D effect but may cause visual discomfort. The minimum setting is 0 (no 3D effect) and the maximum setting is 20 (strong 3D effect).
-------------------------------------
Getter Method
Signature
ParallaxFactor
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParallaxFactor
Parameters: parallaxFactor (int) – New in version NX9.0.0.
License requirements: None.
SupportStereo¶
-
SessionVisualizationSpecialEffects.
SupportStereo
¶ Returns the support stereo flag.
Queries whether your system supports stereo display (A supported graphics card is installed and the Stereo option in hardware vendor control panel is turned on). To see correct stereo display, you also need a 3D Stereo Display or Projector, and 3D glasses (and possibly a hub).
-------------------------------------
Getter Method
Signature
SupportStereo
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.