SessionVisualizationShade Class¶
Properties¶
Property | Description |
---|---|
EdgesEmphasis | Returns or sets the edge emphasis flag. |
LwrtStudioDisplay | Returns or sets the lwrt studio display flag. |
ShowFacetEdges | Returns or sets the show facet edge flag. |
Methods¶
Method | Description |
---|---|
RegenerateShadedViewsFromToleranceChange | Regenerates Shaded Views. |
RegenerateStudioAnalysisViewsFromTolChange | Regenerates Studio Analysis Views. |
Property Detail¶
EdgesEmphasis¶
-
SessionVisualizationShade.
EdgesEmphasis
¶ Returns or sets the edge emphasis flag.
Alters how edges are displayed when Shaded Face Edges is flag is true.
-------------------------------------
Getter Method
Signature
EdgesEmphasis
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgesEmphasis
Parameters: edgesEmphasis (bool) – Edge Emphasis Option to be set or not New in version NX3.0.0.
License requirements: None.
LwrtStudioDisplay¶
-
SessionVisualizationShade.
LwrtStudioDisplay
¶ Returns or sets the lwrt studio display flag.
Alters how studio are displayed.
-------------------------------------
Getter Method
Signature
LwrtStudioDisplay
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LwrtStudioDisplay
Parameters: lwrtStudioDisplay (bool) – Option to be set or not New in version NX4.0.0.
License requirements: None.
ShowFacetEdges¶
-
SessionVisualizationShade.
ShowFacetEdges
¶ Returns or sets the show facet edge flag.
Toggles the display of facet edges. If this flag is true it can help when trying to evaluate or interpret faceted edges.
-------------------------------------
Getter Method
Signature
ShowFacetEdges
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowFacetEdges
Parameters: facetEdges (bool) – New in version NX3.0.0.
License requirements: None.
Method Detail¶
RegenerateShadedViewsFromToleranceChange¶
-
SessionVisualizationShade.
RegenerateShadedViewsFromToleranceChange
¶ Regenerates Shaded Views.
Updates all objects based on their surfacing tolerance.
Signature
RegenerateShadedViewsFromToleranceChange()
New in version NX3.0.0.
Deprecated since version NX12.0.0: Use
NXOpen.Preferences.PartVisualizationShade.RegenerateShadedViewsFromToleranceChange()
instead.License requirements: None.
RegenerateStudioAnalysisViewsFromTolChange¶
-
SessionVisualizationShade.
RegenerateStudioAnalysisViewsFromTolChange
¶ Regenerates Studio Analysis Views.
Updates all objects based on their surfacing tolerance.
Signature
RegenerateStudioAnalysisViewsFromTolChange(updateEnvOption)
Parameters: updateEnvOption (bool) – Send TRUE if env cube updation is required. Else send FALSE New in version NX3.0.0.
Deprecated since version NX12.0.0: Use
NXOpen.Preferences.PartVisualizationShade.RegenerateStudioAnalysisViewsFromToleranceChange()
instead.License requirements: None.