SessionVisualizationScreenViewTriadLocation Enumeration¶
NXOpen.Preferences.SessionVisualizationScreen.ViewTriadLocation is an alias for NXOpen.Preferences.SessionVisualizationScreenViewTriadLocation
-
class
NXOpen.Preferences.
SessionVisualizationScreenViewTriadLocation
¶ Bases:
object
The view triad location types.
Deprecated since version NX12.0.0: Use
NXOpen.Preferences.PartVisualizationScreenViewTriadLocation
insteadEnum Members
Enum Member Enum Member Description BottomLeft View triad display on the bottom left of the view BottomRight View triad display on the bottom right of the view -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-