SessionVisualizationHighQualityImageResolutionType Enumeration¶
NXOpen.Preferences.SessionVisualizationHighQualityImage.ResolutionType is an alias for NXOpen.Preferences.SessionVisualizationHighQualityImageResolutionType
-
class
NXOpen.Preferences.
SessionVisualizationHighQualityImageResolutionType
¶ Bases:
object
The resolution to use when generating a High Quality Image.
Enum Members
Enum Member Enum Member Description Draft Low Medium High UserDefined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-