SessionVisualizationHighQualityImagePlotQualityType Enumeration

NXOpen.Preferences.SessionVisualizationHighQualityImage.PlotQualityType is an alias for NXOpen.Preferences.SessionVisualizationHighQualityImagePlotQualityType

class NXOpen.Preferences.SessionVisualizationHighQualityImagePlotQualityType

Bases: object

Describes the quality desired when plotting the High Quality Image

Enum Members

Enum Member Enum Member Description
Fine
Medium
Rough
Coarse
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.