SessionVisualizationHighQualityImageImageSizeType Enumeration

NXOpen.Preferences.SessionVisualizationHighQualityImage.ImageSizeType is an alias for NXOpen.Preferences.SessionVisualizationHighQualityImageImageSizeType

class NXOpen.Preferences.SessionVisualizationHighQualityImageImageSizeType

Bases: object

The size at which to generate a High Quality Image.

Enum Members

Enum Member Enum Member Description
FillView
AnsiA
AnsiB
AnsiC
AnsiD
AnsiE
IsoA4
IsoA3
IsoA2
IsoA1
IsoA0
UserDefined
TrueSize
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.