SessionVisualizationColorSetting Class¶
-
class
NXOpen.Preferences.
SessionVisualizationColorSetting
¶ Bases:
object
Represents the set of visualization preferences applicable to entire session
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX3.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.PartVisualizationColorSetting
instead.
Properties¶
Property | Description |
---|---|
HandlesColor | Returns or sets the handles color. |
Methods¶
Property Detail¶
HandlesColor¶
-
SessionVisualizationColorSetting.
HandlesColor
¶ Returns or sets the handles color.
Sets the handle color. Unigraphics NX displays all handles using a “handle” color. A session attribute determines the color of handles and applies to all parts in a session.
This property is deprecated. Use
NXOpen.Preferences.PartVisualizationColorSetting.HandleColor`()
instead.-------------------------------------
Getter Method
Signature
HandlesColor
Returns: Return type: int New in version NX3.0.0.
Deprecated since version NX7.5.0: Use
NXOpen.Preferences.PartVisualizationColorSetting.HandleColor`()
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
HandlesColor
Parameters: handlesColor (int) – New in version NX3.0.0.
Deprecated since version NX7.5.0: Use
NXOpen.Preferences.PartVisualizationColorSetting.HandleColor`()
insteadLicense requirements: None.