SessionUserInterface Class¶
-
class
NXOpen.Preferences.
SessionUserInterface
¶ Bases:
object
Represents the set of User Interface preferences applicable to entire session.
Other User Interface settings are available with
NXOpen.Preferences.PartUserInterface
for settings applicable to part and with the SessionUserInterfaceUI class for UI based User Interface Preferences To obtain an instance of this class, refer toNXOpen.Preferences.SessionPreferences
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
InsetMenuDialogComments | Returns or sets the insert menu/dialog comments flag |
JournalFileFormat | Returns or sets the journal file format |
JournalLanguage | Returns or sets the journal language. |
Methods¶
Enumerations¶
SessionUserInterfaceJournalFileFormatType Enumeration | Describes the available format types for a journal file |
SessionUserInterfaceJournalLanguageType Enumeration | Describes the language used to record journals |
Property Detail¶
JournalFileFormat¶
-
SessionUserInterface.
JournalFileFormat
¶ Returns or sets the journal file format
-------------------------------------
Getter Method
Signature
JournalFileFormat
Returns: Return type: NXOpen.Preferences.SessionUserInterfaceJournalFileFormatType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
JournalFileFormat
Parameters: journalFileFormat ( NXOpen.Preferences.SessionUserInterfaceJournalFileFormatType
) –New in version NX3.0.0.
License requirements: None.
JournalLanguage¶
-
SessionUserInterface.
JournalLanguage
¶ Returns or sets the journal language.
Setting the journal language to C++ restricts the file format to Ascii.
-------------------------------------
Getter Method
Signature
JournalLanguage
Returns: Return type: NXOpen.Preferences.SessionUserInterfaceJournalLanguageType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
JournalLanguage
Parameters: language ( NXOpen.Preferences.SessionUserInterfaceJournalLanguageType
) –New in version NX3.0.0.
License requirements: None.