SessionSketchBackgroundType Enumeration¶
NXOpen.Preferences.SessionSketch.BackgroundType is an alias for NXOpen.Preferences.SessionSketchBackgroundType
-
class
NXOpen.Preferences.
SessionSketchBackgroundType
¶ Bases:
object
Describes the available sketch background types.
Enum Members
Enum Member Enum Member Description Inherit Sketch background color is inherited from the parent application Plain Sketch background color is forced to the plain background color -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-