SessionPdmUnpopulatedBehaviourType Enumeration

NXOpen.Preferences.SessionPdm.UnpopulatedBehaviourType is an alias for NXOpen.Preferences.SessionPdmUnpopulatedBehaviourType

class NXOpen.Preferences.SessionPdmUnpopulatedBehaviourType

Bases: object

Options for when to add NX datasets upon loading an unpopulated part in the PDM system

Enum Members

Enum Member Enum Member Description
OnSave
ModifiedPrompt
ModifiedNoPrompt
Never
PreNx4
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.