SessionModelingSurfaceExtensionOption Enumeration

NXOpen.Preferences.SessionModeling.SurfaceExtensionOption is an alias for NXOpen.Preferences.SessionModelingSurfaceExtensionOption

class NXOpen.Preferences.SessionModelingSurfaceExtensionOption

Bases: object

Options for controling how surfaces will be extended while moving geometry

Enum Members

Enum Member Enum Member Description
Linear
Soft
Reflective
Natural
Arc
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.