SessionModelingSaveDataForFeatureEditOption Enumeration¶
NXOpen.Preferences.SessionModeling.SaveDataForFeatureEditOption is an alias for NXOpen.Preferences.SessionModelingSaveDataForFeatureEditOption
-
class
NXOpen.Preferences.
SessionModelingSaveDataForFeatureEditOption
¶ Bases:
object
Options for controling what additional data needs to be saved in part file to enhance the feature edit
Enum Members
Enum Member Enum Member Description NotSet Indicates the no additional data is saved FastRollback Indicates the additional parasolid data is saved for faster rollback FastRollbackAndPreviousStateOfFailedFeature Indicates the additional parasolid data is saved for faster rollback and to show the previous state of failed feature -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-