SessionModelingPolylineStyleType Enumeration

NXOpen.Preferences.SessionModeling.PolylineStyleType is an alias for NXOpen.Preferences.SessionModelingPolylineStyleType

class NXOpen.Preferences.SessionModelingPolylineStyleType

Bases: object

Styles for polylines of B curves and B surfaces

Enum Members

Enum Member Enum Member Description
Solid
Dashed
Phantom
Centerline
Dotted
Longdashed
Dotteddashed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.