SessionModelingImmediateChildrenType Enumeration¶
NXOpen.Preferences.SessionModeling.ImmediateChildrenType is an alias for NXOpen.Preferences.SessionModelingImmediateChildrenType
-
class
NXOpen.Preferences.
SessionModelingImmediateChildrenType
¶ Bases:
object
Describes whether the Immediate Children type is selected for first level or for all
Enum Members
Enum Member Enum Member Description FirstLevel Indicates that Immediate Children type is at first level All Indicates that Immediate Children type is at all level -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-