SessionModelingFreeFormConstructionResultType Enumeration¶
NXOpen.Preferences.SessionModeling.FreeFormConstructionResultType is an alias for NXOpen.Preferences.SessionModelingFreeFormConstructionResultType
-
class
NXOpen.Preferences.
SessionModelingFreeFormConstructionResultType
¶ Bases:
object
Describes whether the Free Form Construction Result is plane or B Surface
Enum Members
Enum Member Enum Member Description Plane Indicates the construction result option is plane BSurface Indicates the construction result option is B Surface -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-