SessionModelingEndpointDisplayStyleType Enumeration

NXOpen.Preferences.SessionModeling.EndpointDisplayStyleType is an alias for NXOpen.Preferences.SessionModelingEndpointDisplayStyleType

class NXOpen.Preferences.SessionModelingEndpointDisplayStyleType

Bases: object

Styles for display endpoints of curves

Enum Members

Enum Member Enum Member Description
OpenCircle
FilledCircle
PlusSign
Cross
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.