SessionModelingBooleanFacePropertiesInheritance Enumeration¶
NXOpen.Preferences.SessionModeling.BooleanFacePropertiesInheritance is an alias for NXOpen.Preferences.SessionModelingBooleanFacePropertiesInheritance
-
class
NXOpen.Preferences.
SessionModelingBooleanFacePropertiesInheritance
¶ Bases:
object
Describes whether the display of Boolean Face properties inherits from target body or tool body
Enum Members
Enum Member Enum Member Description TargetBody Indicates that display of boolean face properties inherits from target body ToolBody Indicates that display of boolean face properties inherits from tool body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-