SessionModelingBodyTypeOption Enumeration¶
NXOpen.Preferences.SessionModeling.BodyTypeOption is an alias for NXOpen.Preferences.SessionModelingBodyTypeOption
-
class
NXOpen.Preferences.
SessionModelingBodyTypeOption
¶ Bases:
object
Describes whether the body type is solid or sheet
Enum Members
Enum Member Enum Member Description Solid Indicates Body Type is solid Sheet Indicates Body Type is solid -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-