SessionDraftingEdgeFaceDisplayType Enumeration

NXOpen.Preferences.SessionDrafting.EdgeFaceDisplayType is an alias for NXOpen.Preferences.SessionDraftingEdgeFaceDisplayType

class NXOpen.Preferences.SessionDraftingEdgeFaceDisplayType

Bases: object

Describes the available edge face display types

Enum Members

Enum Member Enum Member Description
DisplayAndEmphasize
CurvesOnly
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.