SessionAssembliesPositioningTaskCollectionOptionForDesignElements Enumeration

NXOpen.Preferences.SessionAssemblies.PositioningTaskCollectionOptionForDesignElements is an alias for NXOpen.Preferences.SessionAssembliesPositioningTaskCollectionOptionForDesignElements

class NXOpen.Preferences.SessionAssembliesPositioningTaskCollectionOptionForDesignElements

Bases: object

Specify whether Design Elements will be added to the Work or Context Collection of a Positioning Task

Enum Members

Enum Member Enum Member Description
Work
Context
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.