SessionAssembliesPartNameOption Enumeration

NXOpen.Preferences.SessionAssemblies.PartNameOption is an alias for NXOpen.Preferences.SessionAssembliesPartNameOption

class NXOpen.Preferences.SessionAssembliesPartNameOption

Bases: object

Describe whether the part name style is file name or description or specified

Enum Members

Enum Member Enum Member Description
FileName
Description
SpecifiedAttributes
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.