RoutingPathRadiusUnits Enumeration¶
NXOpen.Preferences.RoutingPath.RadiusUnits is an alias for NXOpen.Preferences.RoutingPathRadiusUnits
-
class
NXOpen.Preferences.
RoutingPathRadiusUnits
¶ Bases:
object
Describes units of specified radius value
NXOpen.Preferences.RoutingPathRadiusMethod.Radius
only.Enum Members
Enum Member Enum Member Description NotSet Unspecified. Use units of part file. Inches Use inch units Millimeters Use metric (mm) units -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-