RoutingPathDefaultCornerType Enumeration¶
NXOpen.Preferences.RoutingPath.DefaultCornerType is an alias for NXOpen.Preferences.RoutingPathDefaultCornerType
-
class
NXOpen.Preferences.
RoutingPathDefaultCornerType
¶ Bases:
object
Describes the types of corners allowed in a routing application.
Enum Members
Enum Member Enum Member Description NotSet No Corner Bend Bend Corner Miter Miter Corner BendTable Not really a corner type. Used to indicate use of bend table in conjunction with a Bend corner -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-