RoutingPathChainMethod Enumeration¶
NXOpen.Preferences.RoutingPath.ChainMethod is an alias for NXOpen.Preferences.RoutingPathChainMethod
-
class
NXOpen.Preferences.
RoutingPathChainMethod
¶ Bases:
object
Path curve chaining methods
Enum Members
Enum Member Enum Member Description NoBranch Curves must be mono-connected Continuous Tangents must match at each connection Tangent Use curve with closest tangent when searching Cycle Return all chains MinDist Chain with minimum path length MaxDist Chain with maximum path length -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-