RoutingPathAllowedCornerType Enumeration¶
NXOpen.Preferences.RoutingPath.AllowedCornerType is an alias for NXOpen.Preferences.RoutingPathAllowedCornerType
-
class
NXOpen.Preferences.
RoutingPathAllowedCornerType
¶ Bases:
object
Describes the types of corners allowed in a routing application.
Enum Members
Enum Member Enum Member Description NotSet UF_ROUTE_AV_CORNERS_NONE Bend UF_ROUTE_AV_CORNERS_BEND Cope UF_ROUTE_AV_CORNERS_COPE Miter UF_ROUTE_AV_CORNERS_MITER Sbend UF_ROUTE_AV_CORNERS_SBEND -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-