RoutingPathAddPointsToSpline Enumeration¶
NXOpen.Preferences.RoutingPath.AddPointsToSpline is an alias for NXOpen.Preferences.RoutingPathAddPointsToSpline
-
class
NXOpen.Preferences.
RoutingPathAddPointsToSpline
¶ Bases:
object
Should points be added to existing spline when they are subdivided to preserve shape?
Enum Members
Enum Member Enum Member Description False Do not merge duplicate RCPs. True Merge duplicate RCPs. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-