RoutingPartStockLengthDisplay Enumeration¶
NXOpen.Preferences.RoutingPart.StockLengthDisplay is an alias for NXOpen.Preferences.RoutingPartStockLengthDisplay
-
class
NXOpen.Preferences.
RoutingPartStockLengthDisplay
¶ Bases:
object
The stock length display options available for the Routing bill of material.
Enum Members
Enum Member Enum Member Description Sum Display single sum for each type of stock. Item Display length of each stock individually. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-