RoutingPartPreferredPortMethod Enumeration¶
NXOpen.Preferences.RoutingPart.PreferredPortMethod is an alias for NXOpen.Preferences.RoutingPartPreferredPortMethod
-
class
NXOpen.Preferences.
RoutingPartPreferredPortMethod
¶ Bases:
object
Available methods for determining which port is the preferredport during calculation of placement solutions.
Enum Members
Enum Member Enum Member Description Attribute Examine an attribute applied to the port, and match it’s value to a desired value. Name Compare the ports name with a desired value. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-